FB#.MULTITURNBITS
Description
Number of multi-turn bits used for BiSS
"Bi-directional Serial Synchronous interface"
An open-source communication protocol for feedback devices. With BiSS, all of the computation for interpolation in regard to position occurs on the ASIC directly in the encoder encoders when used in rotary motors. This is specified by the feedback datasheet.
Context
Only used when FB#.MECHTYPE is rotary and identified feedback is BiSS. See Feedback # View.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
multi-turn bits |
|
Range |
0 to 32 |
|
Default Value |
12 |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
|
|---|---|---|---|---|---|---|---|
|
FB1.MULTITURNBITS |
3500h |
0ch |
Unsigned8 |
- |
- |
Read/Write |
No |
|
FB2.MULTITURNBITS |
3501h |
0ch |
Unsigned8 |
- |
- |
Read/Write |
No |
|
FB3.MULTITURNBITS |
3502h |
0ch |
Unsigned8 |
- |
- |
Read/Write |
No |
|
FB4.MULTITURNBITS |
3503h |
0ch |
Unsigned8 |
- |
- |
Read/Write |
No |
|
FB5.MULTITURNBITS |
3504h |
0ch |
Unsigned8 |
- |
- |
Read/Write |
No |
|
Name |
ID |
Hex |
Data Type |
Access |
Units |
|---|---|---|---|---|---|
|
FB1.MULTITURNBITS |
30340 |
7684 |
Unsigned8 |
Read/Write |
- |
|
FB2.MULTITURNBITS |
30341 |
7685 |
Unsigned8 |
Read/Write |
- |
|
FB3.MULTITURNBITS |
30342 |
7686 |
Unsigned8 |
Read/Write |
- |
|
FB4.MULTITURNBITS |
30343 |
7687 |
Unsigned8 |
Read/Write |
- |
|
FB5.MULTITURNBITS |
30344 |
7688 |
Unsigned8 |
Read/Write |
- |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
FB1.MULTITURNBITS |
30340 |
Unsigned8 |
Read/Write |
- |
|
FB2.MULTITURNBITS |
30341 |
Unsigned8 |
Read/Write |
- |
|
FB3.MULTITURNBITS |
30342 |
Unsigned8 |
Read/Write |
- |
|
FB4.MULTITURNBITS |
30343 |
Unsigned8 |
Read/Write |
- |
|
FB5.MULTITURNBITS |
30344 |
Unsigned8 |
Read/Write |
- |